- No : 21693
- Release Date : 2018/08/22 16:28
-
Print
PU operation
I am using the inverter in the PU operation mode.
When I press the "RUN" key on the operation panel, the inverter rotates forward. How can I have it rotate in reverse when I press the "RUN" key?
- Category :
-
Answer
Set Pr.40 (RUN key rotation direction selection) to "1" (Reverse).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ