• No : 21759
  • Release Date : 2018/08/22 16:29
  • Print

NET mode

I want to use the CC-Link optional card FR-A7NC to implement CC-Link communication, but the inverter does not enter the NET mode.
I set Pr.340 (Communication startup mode selection) to "10", and Pr.79 (Operation mode) to "2".
What else should I do?
Category : 

Answer

After setting Pr.340 to "10", you need to power OFF then ON the inverter to make the new setting enabled because you are setting the operation upon power-on.

Power OFF then ON the inverter.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700