• No : 21827
  • Release Date : 2018/08/22 16:29
  • Print

CC-Link

In CC-Link operation, I want to input the inverter's operation status into the programmable controller.
I want to monitor the running frequency, output current value, and conveyor speed simultaneously.
Category : 

Answer

You cannot monitor the running frequency and conveyor speed (machine speed) simultaneously.
The inverter does not have a function to output them simultaneously.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700