- No : 21828
- Release Date : 2018/08/22 16:29
-
Print
CC-Link
I consider performing CC-Link operation. Can the operation (start) commands be input both from PU and NET?
- Category :
-
Answer
The start commands cannot be input from both sources simultaneously because the operation command source is specified.
You can switch the command source as necessary.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700