- No : 21839
- Release Date : 2018/08/22 16:29
-
Print
CC-Link
Where can I set the station number and baud rate?
I want to set the baud rate to 10 Mbps.
- Category :
-
Answer
Use Pr.542 to set the station number and Pr.543 to set the baud rate.
To set the baud rate to 10 Mbps, set Pr.543 to "4".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700