- No : 21873
- Release Date : 2018/08/22 16:29
-
Print
CC-Link
In CC-Link operation, how many inverters can be connected to a single CC-Link system master at maximum?
- Category :
-
Answer
Up to 42 units can be connected. (When only inverters are connected)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700