• No : 21883
  • Release Date : 2018/08/22 16:29
  • Print

Frequency

When using Y100D (frequency setting command RAM) to continuously change the frequency in the sample program for CC-Link, is it necessary to keep Y100D turned ON?
Category : 

Answer

Keep Y100D turned ON if you are changing the frequency continuously. 
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700