- No : 22090
- Release Date : 2018/08/22 16:30
-
Print
Phase detection terminal
I cannot find the terminal block for the FR-RC-15K's phase detection terminal.
Where is the phase detection terminal (TB1-5)?
I found all other terminals.
- Category :
-
Answer
The phase detection terminal has been provided with units produced since December 1999.
You can identify these units with the serial number "N9Z○○○○○○" or later.
"N" is a symbol for the unit, "9" following it represents the year 1999, and "Z" represents December.
If your unit does not have the phase detection terminal, use the conventional wiring method.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Power regeneration converter
- Series
- Option