• No : 22137
  • Release Date : 2018/08/27 16:41
  • Update : 2018/09/07 12:43
  • Print

As to logging period of the internal memory of the main unit.

How long is the logging period of the internal memory of the main unit?
Category : 

Answer

Logging period of the internal memory of the main unit as following:
1. In case of detailed data
Logging period differs according to logging cycle for detail data and the number of measuring circuits.


2. In case of 1hour data
Logging period differs according to the number of measuring circuits.

* It is the logging period where data is output at maximum volume.
Product Name
Energy Measuring Units
Series
EcoMonitor Plus, EcoMonitorLight