As the parameter settings of the FX3 intelligent function modules are not supported by GX Works3,
they cannot be selected from the element selection window.
Please use the configure using the program.
Also, regarding the setting and programming , please refer to the corresponding manual of each FX3 intelligent function modules.