FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-Q Series
>
Settings of the built-in Ethernet port of the universal model QCPU
Back
No : 22618
Release Date : 2018/09/03 17:29
Update : 2018/09/21 10:06
Print
Settings of the built-in Ethernet port of the universal model QCPU
Where can I make settings of the built-in Ethernet port of a universal model QCPU?
Category :
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-Q Series
Answer
Make settings of the built-in Ethernet port in the [Built-in Ethernet Port Setting] tab of the PLC parameter
in GX Works2 or GX Developer.
Product Name
MELSEC-Q Series
Series
CPU