• No : 22618
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/21 10:06
  • Print

Settings of the built-in Ethernet port of the universal model QCPU

Where can I make settings of the built-in Ethernet port of a universal model QCPU?
Category : 

Answer

Make settings of the built-in Ethernet port in the [Built-in Ethernet Port Setting] tab of the PLC parameter
in GX Works2 or GX Developer.
Product Name
MELSEC-Q Series
Series
CPU