- No : 22689
- Release Date : 2018/09/03 17:29
-
Print
Update timing of QD75 current feed value and machine feed value
When are the current feed value and the machine feed value of QD75P1/P2/P4/D1/D2/D4 updated?
- Category :
-
Answer
The values are updated at the timing described below.
- Current feed value: 1.8 ms
- Machine feed value: 56.8 ms
- Product Name
- MELSEC-Q Series
- Series
- Positioning Module