- No : 22703
- Release Date : 2018/09/03 17:29
-
Print
Error code "2400" in QCPU
The error code "2400" has occurred in QCPU.
The Parameter No. under Individual Error Information is "7000H". Are there any remedies?
- Category :
-
Answer
The error code "2400" is "FILE SET ERROR".
It may be determined as the cause of the error that the file that has been specified by a parameter does not exist.
The individual information parameter number "7000H" corresponds to the program setting.
Check that the program that has been set by the program setting matches the program that has been stored in the CPU module.
- Product Name
- MELSEC-Q Series
- Series
- Q (Q mode)