- No : 22806
- Release Date : 2018/09/03 17:30
-
Print
LCPU built-in I/O function
What function does LCPU built-in I/O function provide?
Is it possible to use it for general-purpose I/O function or high-speed counter function?
- Category :
-
Answer
The built-in I/O functions are standard functions of the L series CPU. Combining these functions flexibly achieves various controls with lower cost, eliminating the need for dedicated modules for each function.
The output type of the built-in I/O (function) is selectable between sink type and source type.
For more details, refer to "MELSEC-L CPU Module User's Manual (Built-In I/O Function)".
- Product Name
- MELSEC-L Series
- Series
- CPU