- No : 22992
- Release Date : 2018/09/03 17:31
-
Print
Buffer memory addresses of CC-Link modules
I want to write and read data using FROM/TO instructions in CC-Link communication. Does each station number have fixed buffer memory addresses for them to be assigned?
- Category :
-
Answer
If the remote net Ver.1 mode is used, each station number is given fixed buffer memory addresses.
If the remote net Ver.2 mode is used, different buffer memory addresses are given according to the type of slave station and the number of points the slave station takes.
- Product Name
- Network Related Products
- Series
- CC-Link