- No : 23041
- Release Date : 2018/09/03 17:31
-
Print
Order in which a CC-Link master module and slave stations are connected
Is it possible to establish a CC-Link network in which a master station is positioned in the center and slave stations are connected at both right and left hand sides of the master module?
- Category :
-
Answer
There is no restriction on the positions of a master station and slave stations where they are connected. (Stations are not required to be connected in order of station number.) Hence connections can be made in a way that puts a master station in the center.
- Product Name
- Network Related Products
- Series
- CC-Link