- No : 23719
 
      - Release Date : 2018/09/19 17:16
 
        - 
          
              Print
          
        
 
  
 
Combination transformer
    
      Is there a distance limitation between MPD-3 type ZVT and a relay? 
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    It is required that the resistance is lower than 5 ohm for a go and return length using sealed cables. Other than MPD-3 type ZVT, it is similar to the distance between MZT type ZCT and a relay. 
  
    
      
        - Product Name
 
          - Protection Relay
 
      
      
        - Series
 
          - MELPRO-A Series