• No : 39303
  • Release Date : 2023/01/12 17:13
  • Print

Regarding display of FX5-ENET/IP in a Module configuration Diagram

In the Module configuration diagram of GX Works3, FX5-ENET/IP is not displayed, do I need to set something?
Category : 

Answer

Please update GX Works3 to the latest version. After updating, FX5-ENET/IP is displayed in the Module configuration diagram of GX Works3.
Download the latest update file from the FA site.
Product Name
FX5-ENET/IP
Product Category
Engineering Software, Network/Communication
Series
MELSEC iQ-F Series