Factory Automation

Solutions

FA Remote

Remote Maintenance

Case.08 Perform maintenance on various FA devices easily, even from Off-site

  • Remote Maintenance
Issues
Perform maintenance on various FA devices easily, even from Off-site
Solution

(1) The VNC server function of the GOT2000 Series enables users to display and operate GOT screens "as is" using a VNC client at remote locations.

(2) Monitor and maintain Mitsubishi Electric devices such as PLCs, servo amplifiers, inverters, robots on GOT screens.

* Using Ewon/Secomea remote solutions, users can easily and safely build a remote access environment.

  • *1 Operations are confirmed with the Ewon Cosy+ and Secomea Sitemanager Series.
  • * Please refer to the relevant product catalog for supported functions and restrictions of each model.
Benefits
  • By linking GOT with individual FA devices, users can review information and perform maintenance using GOT even from remote locations.
  • Possible to minimize the introduction of new devices and introduce remote maintenance.

Product Lineup

Cases