• No : 20816
  • Release Date : 2018/08/22 16:24
  • Print

TH3 terminal of the MT-BR5

There are TH1, TH2, TH3, and E terminals on the control circuit terminal block. What is the TH3 used for?
Category : 

Answer

The resistor unit MT-BR5 manufactured in February 2016 or later has output terminal TH3 (NC contact) as a fault output terminal.
Product Name
Inverter, magnet motor drive
Product Category
Option
Series
Option