- No : 20822
- Release Date : 2018/08/22 16:24
-
Print
Stop-on-contact control of the FR-E700
When the STF is turned OFF while the RT signal and RL signal are on during the stop-on-contact control, does the speed decelerate during the stop-on-contact control?
- Category :
-
Answer
The stop-on-contact control becomes invalid when the start command is turned OFF during the stop-on-contact control and the machine is decelerated to a stop with the speed control.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700