• No : 20822
  • Release Date : 2018/08/22 16:24
  • Print

Stop-on-contact control of the FR-E700

When the STF is turned OFF while the RT signal and RL signal are on during the stop-on-contact control, does the speed decelerate during the stop-on-contact control?
Category : 

Answer

The stop-on-contact control becomes invalid when the start command is turned OFF during the stop-on-contact control and the machine is decelerated to a stop with the speed control.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700