• No : 20823
  • Release Date : 2018/08/22 16:24
  • Print

FR-A800 and Ethernet IP communication

Can the Ethernet IP communication control the FR-A800?
Category : 

Answer

Yes. the options support it. By connecting the following communication option (built-in circuit board) manufactured and sold by HMS to the FR-A800 series, the FR-A800 can be supported by the communication protocol of the Ethernet IP. HMS model: A8NEIP_2PFor the details, please contact your local sales office (sales) or agency.
Product Name
Inverter, magnet motor drive
Product Category
Plug-in option
Series
Option