- No : 20824
- Release Date : 2018/08/22 16:24
- 
          
              Print
          
        
 
FR-A800 "Parameter for the communication setting"
    
      Pr.1300 to 1400 are described as "Parameter for the communication setting". For what communication are these parameters used? 
    
  
    - Category : 
- 
      
    
 
    Answer
  
    These parameters are used for the communication compatible with the communication protocol of the Ethernet IP of the HMS optional circuit board (A8NEIP_2P). 
  
    
      
        - Product Name
- Inverter, magnet motor drive
        - Product Category
- Inverter
        - Series
- FR-A800