• No : 20830
  • Release Date : 2018/08/22 16:24
  • Print

Seamless communication of FR Configurator SW3

The master and remote I/O station of the programmable controller is connected via the MELSECNET and the inverter is connected to the CC-Link unit of remote I/O. With this configuration, is the CC-Link Seamless communication available?
Category : 

Answer

The communication via the MELSECNET is not available.
Product Name
Inverter, magnet motor drive
Product Category
Engineering software
Series
FR Configurator SW3