• No : 20834
  • Release Date : 2018/08/22 16:24
  • Print

S-shape acceleration/deceleration of the FR-D700

When Pr.29 (Acceleration/deceleration pattern selection) is set as S-shape acceleration/deceleration, does the inflection point of S-shape change from Pr.3 to Pr.84 under General-purpose magnetic flux vector control?
Category : 

Answer

It does not change even when General-purpose magnetic flux vector control is performed. Pr.3 is the inflection point of the S-shape.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-D700