• No : 20838
  • Release Date : 2018/08/22 16:24
  • Print

Switching time of the FR-A800 control

With Real sensorless vector control or Vector control, when switching the torque control and speed control by the MC signal, how long does it take to actually switch the control after the signal is changed?
Category : 

Answer

20 ms or less is required to switch the control with the MC signal.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800