- No : 20842
- Release Date : 2018/08/22 16:24
-
Print
FR-HC2
It is described that Pr.10 cannot be written during operation even when Pr.77 = 2, then how can I write it?
- Category :
-
Answer
Perform the writing after turning ON the SOF, or after stopping the FR-HC2 by pressing the STOP button. Wire the RDY signal so that the inverter stops when the error occurs in the FR-HC2.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Option
- Series
- Option