• No : 20843
  • Release Date : 2018/08/22 16:24
  • Print

STOP function of the FR-A800

Is the self-holding of the STOP function released by the OH signal (External thermal relay input)?
Category : 

Answer

No, it is not. It is released by the inverter reset that releases E.OHT.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800