• No : 20847
  • Release Date : 2018/08/22 16:24
  • Print

FR Configurator2

In FR Configurator2, the option of the FR-A8TP is enabled. Why Vector control cannot be selected in the motor setting?
Category : 

Answer

Vector control cannot be selected unless Pr.862 is set to 1. Only the first motor is supported in the motor setting of FR Configurator2.
Product Name
Inverter, magnet motor drive
Product Category
Engineering software
Series
FR Configurator2