• No : 20848
  • Release Date : 2018/08/22 16:24
  • Print

High speed sampling of FR Configurator2

Is the high speed sampling of the graph available when the FR-A800-E is connected via the Ethernet?
Category : 

Answer

High speed sampling is not available. Only the normal sampling is available.
Product Name
Inverter, magnet motor drive
Product Category
Engineering software
Series
FR Configurator2