- No : 20854
- Release Date : 2018/08/22 16:24
-
Print
Amount of heat generated by the FR-V500L
Is the amount of heat generated by the FR-V500L series the same as the one by the FR-A500L series?
- Category :
-
Answer
It is the same as the one by the inverter whose capacity is one-rank higher than the FR-A500L series.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-V500