• No : 20854
  • Release Date : 2018/08/22 16:24
  • Print

Amount of heat generated by the FR-V500L

Is the amount of heat generated by the FR-V500L series the same as the one by the FR-A500L series?
Category : 

Answer

It is the same as the one by the inverter whose capacity is one-rank higher than the FR-A500L series.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-V500