• No : 20857
  • Release Date : 2018/08/22 16:24
  • Print

CC-Link IE Field Basic

When CC-Link IE Field Basic is used, how many FR-A800-E or FR-F800-E can be connected at the maximum?
Category : 

Answer

Up to 64 (slave stations). The number of connectable units differs depending on the master station.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800-E, FR-F800-E