• No : 20859
  • Release Date : 2018/08/22 16:24
  • Print

Built-in PLC function

What causes the error: 2200 (MISSING PARA) in the PLC function?
Category : 

Answer

The error indicates that the parameter setting of the PLC function is not set. It is considered that the PC parameter is not checked when the PC parameter and program are written to the PC.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800