• No : 20869
  • Release Date : 2018/08/22 16:24
  • Print

FR-E700KNC

Is the inverter reset when the power supply +24 is turned ON and OFF to reflect the parameter such as Pr.542 on the condition that on only +24 is input from the external input terminal? 
Category : 

Answer

The inverter is reset.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700