• No : 20875
  • Release Date : 2018/08/22 16:24
  • Print

FR-A8NC

When supplying the 24 VDC power, why can Pr.542 (station number setting) be read without connecting the FR-A8NC?
Category : 

Answer

When the 24 VDC power is supplied, optional parameters can be read.
Product Name
Inverter, magnet motor drive
Product Category
Plug-in option
Series
Option