- No : 20876
- Release Date : 2018/08/22 16:24
-
Print
FR-A8TR
As the restriction of the FR-A8TR, it is described that the terminals +24, 10E, 4, and STOP are unavailable when the FR-A8NC is used. What is the reason for that?
- Category :
-
Answer
Because when the FR-A8NC and FR-A8TR are used together, the wiring to the terminals becomes physically difficult.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- Option