• No : 20878
  • Release Date : 2018/08/22 16:24
  • Print

FR-A800

Do the metallic sound of the motor and leakage current at the offline auto tuning change according to the value of Pr.72 (PWM frequency selection)?
Category : 

Answer

No, they do not. Pr.72 is invalid at the offline auto tuning. It is also invalid when the motor rotates with Pr.96 = 101.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800