• No : 20879
  • Release Date : 2018/08/22 16:24
  • Print

FR-A800-E

What type of connection path is used for FR Configurator2?
Category : 

Answer

The direct connection with the inverter like the standard model, and the connection via the GOT and relay station (programmable controller) are available. Only Q and L series are supported by the connection via the programmable controller. (The R series is also supported from Ver.1.10L)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800-E, FR-F800-E