• No : 20884
  • Release Date : 2018/08/22 16:24
  • Print

FR-A800-E

Can the same options as the FR-A800 (RS-485 communication type) be used for the FR-A800-E?
Category : 

Answer

There are some restrictions compared to the FR-A800 (RS-485 communication type). For example, the FR-A8TR is unavailable, and only two option connectors are unoccupied.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800-E, FR-F800-E