• No : 20890
  • Release Date : 2018/08/22 16:24
  • Print

FR-A800-R2R

Can I operate the winding diameter calculation function without a sensor or encoder?
Category : 

Answer

The encoder feedback is always required for the thickness calculation function. The actual line speed calculation function requires the input of the actual line speed. For the actual line speed calculation, the encoder feedback is not required.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800-R2R