- No : 20897
- Release Date : 2018/08/22 16:24
- 
          
              Print
          
        
 
FR-A800
    
      When tuning the SF-V5RU by Pr.71 = 33, does the tuning result change between Pr.9 = 0 and Pr.9 = Rated motor current setting? 
    
  
    - Category : 
- 
      
    
 
    Answer
  
    Yes. When Pr.9 = 0, turning is performed with the inverter rated current. 
Always set the rated motor current. 
  
    
      
        - Product Name
- Inverter, magnet motor drive
        - Product Category
- Inverter
        - Series
- FR-A800