• No : 20899
  • Release Date : 2018/08/22 16:24
  • Print

Terminal response time

What is the terminal response time of the FR-A800? Can I adjust the terminal response time so that it becomes equal between before and after the replacement from the A700 series?
Category : 

Answer

It is 2 to 3 ms. By setting Pr.289 Inverter output terminal filter and Pr.699 Input terminal filter, the FR-A700 can be compatible with the response of the terminals of the FR-A700. Adjust it according to the system with a guide of 5 to 8 ms.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800