• No : 20903
  • Release Date : 2018/08/22 16:25
  • Print

Carrier frequency automatic reducing function

Does the carrier frequency automatic reduction function of Pr.260 operate immediately?
Category : 

Answer

The function operates immediately when the current of 85% or higher flows. The limit is canceled when the current becomes 80% or lower.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800