- No : 20915
- Release Date : 2018/08/22 16:25
-
Print
Monitoring function of the FR-A800-R2R
Can the monitoring function of the terminal 1 input voltage and the terminal 1 after calibration (%) be monitored when Pr.363 is other than "5"?
- Category :
-
Answer
No, they cannot be monitored when Pr.363 is other than "5". They are enabled only when Pr.363 = 5.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800 Plus