- No : 20922
- Release Date : 2018/08/22 16:25
-
Print
FR-A800-GF
Can the same options as the FR-A800 be used for the FR-A800-GF?
- Category :
-
Answer
Yes, the options are the same as the FR-A800 standard model. Note that two options can be added at maximum. (One option is already used as standard.) Other communication options are unavailable.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800