- No : 20936
- Release Date : 2018/08/22 16:25
-
Print
FR-F800
Can Pr.22, the stall prevention function, limit the current under the PM sensorless control when the MM-EFS is controlled by the F800?
- Category :
-
Answer
Yes, the current is limited under the PM sensorless control.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-F800