- No : 20941
- Release Date : 2018/08/22 16:25
-
Print
FR-HC2
Does the inverter stop when the SOF signal of the HC2 is turned ON?
- Category :
-
Answer
The internal transistor of the HC2 stops by turning on the SOF signal and stopping the converter. As a result, regenerative driving is not performed. However, the test run of the inverter with no load can be performed because the voltage output between P and N is not shut off. (Since the main circuit capacitor or others of the HC2 generates heat, the normal operation to which a load is applied cannot be performed.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Option
- Series
- Option